:CALCulate:TRACe{Tr}:MARKer{Mk}:FUNCtion:EXECute

Type

Command Only

Syntax

:CALCulate:TRACe{Tr}:MARKer{Mk}:FUNCtion:EXECute

Description

This command executes marker Max or Min for a selected marker function. This is different than tracking mode because moving the marker to another point, the marker does not point back to Max or Min that is previously set.

Examples

10 OUTPUT 717;":CALC:TRAC1:MARK1:FUNC:TYPE MAX"
10 OUTPUT 717;":CALC:TRAC1:MARK1:FUNC:EXEC"

Related Commands

:CALCulate:TRACe{Tr}:MARKer{Mk}:FUNCtion:TRACking

:CALCulate:TRACe{Tr}:MARKer{Mk}:FUNCtion:TYPE

Equivalent GUI

No equivalent GUI is available.